xEnergy Configurator
To make it as easy as possible for you to plan and design an xEnergy system, we offer you the proven xEnergy Configurator as a free planning tool.
- Easy to handle when selecting xEnergy components
- Windows-based dialogue guidance
- Functional, self-evident structure
- Short training period thanks to Look and Feel
- Versatile applications
- Project management and system structure
- The function-based system choice automatically generates the suitable distributor
- Generation of a bill of material for steel work, device fitting kits and mainpower devices
- Generation of a front view for providing offers, individual adjustment by Drag and Drop
- Calculation of the copper and of the temperature rise
- Detailed catalogue with Ordering section and Technical Data section
- Guidance thanks to instruction leaflets, set-up instructions and technical manuals
Eaton Configurator
Eaton Configurator material database without pricing information
Download Eaton xEnergy material database file (without pricing information)
Please contact your Eaton representative to request a material database with pricing information.
Eaton Configurator material database with German price information
Download Eaton xEnergy material database file (with German pricing information)
Eaton Configurator material database with Dutch price information
Download Eaton xEnergy material database file (with Dutch pricing information)
Eaton Configurator material database with Belgian price information
Download Eaton xEnergy material database file (with Belgian pricing information)
Eaton Configurator material database with Luxembourg price information
Download Eaton xEnergy material database file (with Luxembourg pricing information)
Eaton Configurator material database with Spanish price information
Download Eaton xEnergy material database file (with Spanish pricing information)
Eaton Configurator material database with Italian price information
Download Eaton xEnergy material database file (with Italian pricing information)
Empty Eaton Configurator material database
In addition to the standard Eaton material database, a user material database can be used. This makes it possible to create your own material and manage it independently of the standard material database.
Download empty database file for use with user-specific material
Version 2/2020 (R810.3) contains the following improvements.
Highlights:
- With the new update function, available program updates are automatically offered to the user directly within the configurator application.
- It is possible to run the configurator application in 64-bit mode. This requires the 64-bit Microsoft Access Database Engine 2010. Download from microsoft.com
- Increased execution speed when inserting devices.
- The configuration rules and graphics for Modan and xEnergy products have been updated.
- The xEnergy Light system has been completely updated. (Product development package 2)
- The XR Mixed panel has been completely redesigned. If you open a project from a previous version of the Configurator, we recommend that you make a backup copy of the project file. If necessary, the configurator automatically offers to create a backup copy.
- The new product series NZM with PXR electronics has been integrated into the Configurator.
- The new product series Power Defense PDE has been integrated into the Configurator.
- The new mounting modules for the NZM frame size 3 were integrated into the XP distribution panels within the xEnergy Main System (main busbar at the back).
- In the xEnergy Main System (main busbar at the back) a floor plan of the low-voltage switchgear can be output.
- The export of preview graphics to DWG/DXF has been improved.
- The export from the shopping cart to Excel has been improved.
- General bug fixes in the graphics, configuration rules and translations.
Version 1/2020 (R788.9) contains the following improvements.
Highlights:
- The editing speed in large projects has been improved.
- Handling of project files on network drives has been improved.
- A new feature allows to select the installation area within modules when creating a new device. For example: selection of individual DIN rails within EP modules or selection of individual slots in NZM mounting kits.
- Completely updated configuration rules.
- Improvements in the new xEngery Light System.
- Bug fixes in the XR mixed fields.
- Improved export of the shopping cart to Excel.
- General bug fixes in graphics, rules and translations.
Version 2/2019 (R781.2) contains the following improvements.
Highlights:
- The xEnergy Light Configurator has been completely redesigned in line with product updates.
- New graphics for the xEnergy Light Configurator have been created.
- The new xEnergy Light Configurator has been enhanced with the view from the top.
- The product database has been updated to September 2019 (09-2019).
- In the xEnergy Main BXT Configurator the data from the building instructions for the copper busbar calculation have been updated.
- In xEnergy Safety several bugs have been fixed and improvements implemented.
- The Modan S Configurator has been updated.
- In Modan S Configurator it is possible to create German tender texts for the complete low-voltage main distribution.
- In the xEnergy Main Configurator several product updates have been implemented and bugs have been fixed.
Summary of changes and additions with respect to version R756.4:
- The switching capacity option has been removed from the FCFSD and NHW-SLS fuse strips.
- When creating elements, it is ensured that only installation modules appear in which the element can be installed.
- A problem caused by a terminal block has been fixed with the DXF export.
- The duplication of components was further accelerated. Additionally, a message is displayed if there is not enough mounting space available for multiple duplicated components.
- The Update Material function has been enhanced and is also applied to "User Material".
- The English translations have been updated.
- The French translations have been updated.
- The Italian translations have been updated.
- The Dutch translations have been updated.
- The Polish translations have been updated.
- The Russian translations have been updated.
- The Spanish translations have been updated.
- The Czech translations have been updated.
- The Hebrew translations are no longer maintained.
- A printing error has been fixed. The error was caused by text elements in the preview.
- Fixed a problem that caused unintentional changes to existing NZM circuit breakers.
- Added handling of different currencies for metal surcharges. In the dialog "Options shopping cart" the price information with the appropriate currency (as used in the shopping cart) is now set and applied.
- An error has been corrected in the NZM code, the N4 disconnector can also be selected in the withdraw mechanism.
- In the shopping cart the calculation of the prices in the sum list was corrected. With the " Custom material " the discount factors were correctly applied only after a change of the view.
- In the shopping cart a description in the " Sum list distribution board " was corrected. The " Sum list distribution board " displayed the result of the view "Structure" for the sum entries of the project and the distribution board.
- In the xEnergy Basic EP module for Dumeco an error in the graphic of the mounting plate and front plate was fixed.
- In xEnergy Basic EP an error in placing a Dumeco switch was fixed.
- In xEnergy Basic EP a problem with direct placement of Dumeco switches has been fixed.
- In the xEnergy Basic and Light the mounting areas at the top and bottom of the cabinet have been blocked for Profi+ NZM mounting kits.
- In xEnergy Basic and Light new graphics were created for the Power Defense Profi+ installation kit.
- In xEnergy Basic an error when creating "Dummy Subgroup for User Material" was corrected.
- In xEnergy Basic a problem with updating calculated material was fixed. After duplicating or copying and pasting, the number of pieces of material such as APH05, APH, BPZ-TW, EPTV105 is calculated correctly.
- The xEnergy Light displays the ventilation slots in the doors.
- In xEnergy Light an occasional problem with the calculation of side walls has been fixed.
- In xEnergy Light new graphics for the compact circuit-breakers output modules NZM1, NZM2, NZM3 or PD1, PD2, PD3 have been created.
- In xEnergy Light, new graphics have been created for the Power Module NZM3, NZM4, PD3 and PD4 compact circuit-breakers.
- In xEnergy Light, new graphics have been created for the Power Module IZMX16, IZMX40 and PSL2000 circuit-breakers.
- New graphics for the mounting plates and front plates were created in xEnergy Light.
- In the xEnergy Main BBB and BXT the category "Flat copper..." has been preset as default value in the function cutting stock solver.
- In xEnergy Main BBB and BXT the cutouts for the NZM PXR were added.
- In the xEnergy Main BBB the graphic of the roof covers with F3A flanges at 1350mm wide housings was corrected.
- In the xEnergy Main BBB the copper calculation for the BA 181 was corrected.
- In the xEnergy Main BBB, the default value was changed to " Feeder" when directly creating an ACB or MCCB.
- In the xEnergy Main BBB the XF modules " fused " were changed from GSTA to XNH.
- In the xEnergy Main BBB XF section, the article XPLSTB-1000 is automatically added for NH strips.
- In the xEnergy Main BXT the module door for NZM 4 has been locked for the XP sections.
- In xEnergy Main BXT the calculation of the rated operational current for the 12x30/10 main busbar has been updated.
- In the xEnergy Main the bill of materials for the main contacts of the XW plug-in units has been corrected. An error occurred with the setting "Allow mechanical oversize".
- In the xEnergy Main the obsolete checkbox "with devices" was removed.
- In xEnergy Main a faulty dimensioning in the top view was corrected.
- In xEnergy Main the hole diameter of the base and the base frame was dimensioned in the top view.
- In xEnergy Main the new IP55 hoods of the IZM circuit breakers were implemented.
- In the xEnergy Main, new roof covers with cable entries were integrated for passive arc fault protection.
- In the xEnergy Main XP field with 2x NZM4, the arrow for displaying the connection direction was corrected for the door (blind) option.
- In xEnergy Safety, the automatic calculation of flanges on enclosures at the top and bottom of the segment has been extended.
- In xEnergy Safety, an error in the graphic was corrected. CI43 busbar enclosures rotated by 90° were placed outside the segment or changed the positions of existing enclosures.
- In the Profi+ module for NZM1 circuit-breakers, the position of the mounting area was corrected.
- The cover strip for SASY60i has been updated in the component code.
- Integration of Pan Assemblies - MCCB boards in the new xEnergy Light Configurator.
Version 1/2019 (R756.4) contains the following improvements.
Highlights:
- The xEnergy Safety Configurator has been completely revised in line with product updates.
- The product ranges have been updated as of January 2019.
- With the new "Undo" and " Redo" functions, one or more last actions can be undone.
- The memory (RAM) usage of the configurator has been optimized.
- The speed when creating components and duplicating distribution boards has been improved.
- In xEnergy Main it is possible to create German tender texts for the complete low-voltage main distribution.
Summary of changes and additions with respect to version R741:
- When opening old projects, an info message appears. The user can choose to open the project, make a backup copy before opening, or not open the project. In any case, opening the project causes a conversion to the latest version.
- In addition to the function to import a database or license file via drag and drop, new menu items have been created. These menu items can be used to import and manage license files and databases.
- In addition to the standard Eaton material database, a user material database can be used. This makes it possible to create your own material and manage it independently of the standard material database.
- The following measures have significantly improved the use of the Configurator's memory (RAM):
- The Configurator application can use more than 2 GB of memory when used on 64-bit operating systems. The configurator itself remains a 32-bit application for the time being.
- When the Configurator is started, not all xEnergy systems are read in (Basic, Light, Safety, Main). As a result, considerably less RAM is used when the Configurator is started. Only when creating a project with a specific system are the necessary rule set files loaded. In addition, the start time of the Configurator is significantly reduced.
- A separate program instance is used for each open project. By reducing it to one project per instance, the required RAM is limited to this project.
- When creating elements in the Configurator, more memory was used than was actually required for the new elements. The memory requirement is now kept to a minimum even after a new element has been created.
- Unused (e.g. old) material databases are always closed and removed from the RAM.
- No longer needed memory will be released as soon as possible to always have as much memory available as possible.
- The speed of duplicating sections / enclosures and entire distribution boards equipped with components has been improved.
- The speed of component creation has been improved under the following circumstances:
- A module is selected in which there is still sufficient installation space available for the new component.
- A component is selected that is installed in a module in which there is still sufficient installation space available for the new component.
- If the distribution board or the project is selected, either the last element found as installation location or the last selected element is selected.
- If the currently selected element is not suitable for installation, either the last element found as the installation location or the last selected element is selected.
- If a panel / enclosure is selected, it is searched first as before for the installation space.
- The new Multiple Selection option allows multiple elements to be selected together and then deleted or copied and pasted.
- Fixed a bug that caused the location names to be duplicated.
- Fixed an error that occurred when opening a project copy created with the Save As function.
- The incorrect display of the category names "Flat Copper" and "Stabilizer/Supporter" in the shopping cart was corrected.
- In the shopping cart errors with the categories were corrected, by the error articles in the shopping cart were not correctly displayed or hidden.
- When copying graphic or text elements, the relative position of the graphic element to the parent element is now retained when copying the parent element.
- The NZM ruleset has been completely revised, i.e. the order of the properties and the underlying configuration rules have been changed.
- Errors in the settings of the PIFT protection devices have been fixed.
- The parts lists for the current transformers of the NH protection devices FCFSD, NHW and PIFT have been revised.
- In the xEnergy Main XF section a bug in the graphics of the NZM3 with withdrawable AVE was fixed.
- In the xEnergy Main the NH and PIFT sections show the connection direction of the cables.
- In the xEnergy Main the documentation for the busway connections has been updated.
- In the xEnergy Main XR section the configuration rules for the module doors have been corrected.
- In the xEnergy Main XP section the documentation for the IZMX circuit breakers has been updated.
- In xEnergy Basic an error with the calculation of the height indicator in connection with the option "Socket" was fixed.
- The xEnergy Basic and Light mounting kits have been updated for the NZM PXR trip electronics.
- In xEnergy Basic the 4-pole flexible busbar BPZ-KB-24/250 has been added.
- Fixed a preview error in xEnergy Basic and Light that occurred when "DummyMainGroup" and/or "DummySubGroup" were present.
- In xEnergy Light an error with the installation of the N or PE busbar was fixed.
- In xEnergy Light a bug in the preview of the busbar terminals AKU was fixed.
- In the EP installation system, an error with the horizontal and vertical partitions was fixed, the error caused existing installation kits to be moved.
- In the EP installation system an error in the parts list of the EP DIN rail modules was corrected.
- The downsizing of EP and Profi+ DIN modules equipped with components has been improved. The built-in components will be moved to a new DIN module if they can't find space in the smaller module.